TJA1020's RXD does not apear.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

TJA1020's RXD does not apear.

3,388 次查看
Miri
Contributor I

Hello.
I am developing a LIN master board using TJA1020.
In the case of TX, it signals normally and the slave also operates normally.
The problem is that when ID values are sent to receive responses, the response from the slave does not come to RX.
When analyzing the signal of the LIN line, the slave responds normally.
However, there is no signal from the RX pin of the TJA1020.
Please let me know which part I missed.

 

标记 (4)
0 项奖励
回复
1 回复

3,373 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Miri,

Please double check that the TJA1020 is in normal slope mode:

Capture.JPGCapture.JPG

BR, Tomas

0 项奖励
回复