TJA1020's RXD does not apear.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TJA1020's RXD does not apear.

3,673 Views
Miri
Contributor I

Hello.
I am developing a LIN master board using TJA1020.
In the case of TX, it signals normally and the slave also operates normally.
The problem is that when ID values are sent to receive responses, the response from the slave does not come to RX.
When analyzing the signal of the LIN line, the slave responds normally.
However, there is no signal from the RX pin of the TJA1020.
Please let me know which part I missed.

 

Tags (4)
0 Kudos
Reply
1 Reply

3,658 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Miri,

Please double check that the TJA1020 is in normal slope mode:

Capture.JPG

BR, Tomas

0 Kudos
Reply