TJA1020's RXD does not apear.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TJA1020's RXD does not apear.

3,386件の閲覧回数
Miri
Contributor I

Hello.
I am developing a LIN master board using TJA1020.
In the case of TX, it signals normally and the slave also operates normally.
The problem is that when ID values are sent to receive responses, the response from the slave does not come to RX.
When analyzing the signal of the LIN line, the slave responds normally.
However, there is no signal from the RX pin of the TJA1020.
Please let me know which part I missed.

 

タグ(4)
0 件の賞賛
返信
1 返信

3,371件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Miri,

Please double check that the TJA1020 is in normal slope mode:

Capture.JPGCapture.JPG

BR, Tomas

0 件の賞賛
返信