Static bootloader re-request for MC56F8037

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Static bootloader re-request for MC56F8037

1,641件の閲覧回数
laonnuri
Contributor I

Hi, xiangjun_rong

Two weeks ago, you advised me, but I could not generate static_bootloader for MC56F8037 using CodeWarrior for DSP56800Ever8.3 referring to "AN4275.PDF" and "AN3814.PDF".
As the contents of "AN4275.PDF", in MC56F82xx, static_bootloader is created by deleting "#define DYNAMIC" in "File->New->Processor Expert Examples Stationery".
However, only dynamic_bootloader is created in MC56F80xx. Also, the contents of bootloader consist only of source code that deletes all flash_memory using mass_erase when downloading application.


In 2017, you provided static_bootloader source code as shown below, but now I can't download it.

I want a way to create a static_bootloader for the MC56F8037 using codewarrior's "Expert Examples Stationery" or static_booloader_source_code.

qqq.jpg

 

0 件の賞賛
返信
1 返信

1,610件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I attach the two projects, pls check them.

BR

XiangJun Rong

0 件の賞賛
返信