SGTL5000 life span

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,817件の閲覧回数
jan_spurek
NXP Employee
NXP Employee

Hello,

we have a customer who plans to use SGTL5000 and is interested in its life span.

Could you please provide the information?

Best Regards,

Jan

0 件の賞賛
返信
1 解決策
3,648件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Jan,

I have checked the longevity program, the codec SGTL5000 was launched at Jun 2008, it's longevity is 10 year.

Hope it can help you

BR

XiangJun Rong

元の投稿で解決策を見る

4 返答(返信)
3,649件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Jan,

I have checked the longevity program, the codec SGTL5000 was launched at Jun 2008, it's longevity is 10 year.

Hope it can help you

BR

XiangJun Rong

3,648件の閲覧回数
jan_spurek
NXP Employee
NXP Employee

Hello XiangJun Rong,

this is sufficient information. Thank you very much.

Best Regards,

Jan

0 件の賞賛
返信
3,648件の閲覧回数
ani10c89
Contributor II

Hello XiangJun Rong,

Is there any specific date for SGTL5000 discontinuation or it can be still used for new designs.

Our design is aimed at 10 years life support . 

Is there any alternate part for SGTL5000.

Please suggest.

Regards,

Anirudha

0 件の賞賛
返信
3,648件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Anirudha,

I have checked the the following link:

Audio CODEC|NXP 

The state of the chip is "Active", which means that customer can order it via distributor or Buy directly now. The SGTL5000 is Freescale only codec, there is not replacement, because it's longevity is 10 year, now it almost reaches 10 year, so it is not recommended in new design. But we can not give you a date when it will discontinue.

BR

Xiangjun Rong

0 件の賞賛
返信