SGTL5000 life span

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SGTL5000 life span

Jump to solution
3,831 Views
jan_spurek
NXP Employee
NXP Employee

Hello,

we have a customer who plans to use SGTL5000 and is interested in its life span.

Could you please provide the information?

Best Regards,

Jan

0 Kudos
Reply
1 Solution
3,662 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Jan,

I have checked the longevity program, the codec SGTL5000 was launched at Jun 2008, it's longevity is 10 year.

Hope it can help you

BR

XiangJun Rong

View solution in original post

4 Replies
3,663 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Jan,

I have checked the longevity program, the codec SGTL5000 was launched at Jun 2008, it's longevity is 10 year.

Hope it can help you

BR

XiangJun Rong

3,662 Views
jan_spurek
NXP Employee
NXP Employee

Hello XiangJun Rong,

this is sufficient information. Thank you very much.

Best Regards,

Jan

0 Kudos
Reply
3,662 Views
ani10c89
Contributor II

Hello XiangJun Rong,

Is there any specific date for SGTL5000 discontinuation or it can be still used for new designs.

Our design is aimed at 10 years life support . 

Is there any alternate part for SGTL5000.

Please suggest.

Regards,

Anirudha

0 Kudos
Reply
3,662 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Anirudha,

I have checked the the following link:

Audio CODEC|NXP 

The state of the chip is "Active", which means that customer can order it via distributor or Buy directly now. The SGTL5000 is Freescale only codec, there is not replacement, because it's longevity is 10 year, now it almost reaches 10 year, so it is not recommended in new design. But we can not give you a date when it will discontinue.

BR

Xiangjun Rong

0 Kudos
Reply