Refresh While Running in Variables view using DSC MC56F817 doesn't workㄡ

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Refresh While Running in Variables view using DSC MC56F817 doesn't workㄡ

ソリューションへジャンプ
2,230件の閲覧回数
cody1
Contributor III

I add a global variable to the watch view and check "refresh while running". I can not see any thing in the watch view. 

0 件の賞賛
返信
1 解決策
2,218件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Cody,

I do not think that the MC56F817 is a correct part number, pls check and give us the correct part number.

I suppose that you use CodeWarrior for DSP56800E ver8.3 tools to watch variable, in the case, you have to set a break point. When the cpu runs to the break point location, the cpu will halts, then you can see the variable. In conclusion, only after the CPU halts can you watch the variable.

If you do want to watch variable while the CPU is running, you have to use dedicated Freemaster tools, this is Freemaster tools link:

https://www.nxp.com/design/software/development-software/freemaster-run-time-debugging-tool:FREEMAST...

 

BR

Xiangjun Rong

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,219件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Cody,

I do not think that the MC56F817 is a correct part number, pls check and give us the correct part number.

I suppose that you use CodeWarrior for DSP56800E ver8.3 tools to watch variable, in the case, you have to set a break point. When the cpu runs to the break point location, the cpu will halts, then you can see the variable. In conclusion, only after the CPU halts can you watch the variable.

If you do want to watch variable while the CPU is running, you have to use dedicated Freemaster tools, this is Freemaster tools link:

https://www.nxp.com/design/software/development-software/freemaster-run-time-debugging-tool:FREEMAST...

 

BR

Xiangjun Rong

0 件の賞賛
返信