RE: TWR-56F8400 module and JTAG debug module CWH-UTP-ONCE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RE: TWR-56F8400 module and JTAG debug module CWH-UTP-ONCE

2,142 Views
x31
Contributor I

I believe the JTAG debug module CWH-UTP-ONCE that we use with the 56F8367 should work with the TWR-56F8400 - however, the 14 pin header has all 14 pins present whereas the ONCE connector has one pin blocked. Is the ONCE compatible if we cut the corresponding pin?

Labels (1)
0 Kudos
Reply
2 Replies

2,001 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

The CWH-UTP-ONCE device can be used to debug both MC56F83xx and MC56F84xxx, the blocked pin on the JTAG connector of the CWH-UTP-ONCE device is to avoid that the JTAG connector is inserted reversely. The RED line of the 14 pin cable is the pin1 for the CWH-UTP-ONCE device.

Hope it can help you

BR

Xiangjun Rong

2,001 Views
x31
Contributor I

Xiangjun, Thank You.

I have verified the CWH-UTP-ONCE device does work. We cut pin 8 from the JTAG connector.

Len

0 Kudos
Reply