Problem writing code on the MC56F847 DSP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem writing code on the MC56F847 DSP

Jump to solution
1,792 Views
Michell
Contributor I

Hello, I'm having the following problem running the code on the DSP: Error: Couldn't write applet to target. Can not read target memory at location: 0x0000000000000000.Please make sure that the chip selects are properly configured.
The CWPP response code is: CCSProtocolPlugin : CCS: Core not responding.

I'm using the correct settings for the chip because I've been using the same code for weeks, this problem started to happen out of nowhere.

0 Kudos
Reply
1 Solution
1,735 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Can you tell us the part number you are using? There is not MC56F847, maybe it is MC56F84789 or something like that

what is the tools you are using for example CodeWarrior for MVU ver11.x?

Do you use USBTAP or Multilink Universal device?

BR

XiangJun Rong

 

View solution in original post

Tags (1)
0 Kudos
Reply
1 Reply
1,736 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Can you tell us the part number you are using? There is not MC56F847, maybe it is MC56F84789 or something like that

what is the tools you are using for example CodeWarrior for MVU ver11.x?

Do you use USBTAP or Multilink Universal device?

BR

XiangJun Rong

 

Tags (1)
0 Kudos
Reply