Problem writing code on the MC56F847 DSP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem writing code on the MC56F847 DSP

ソリューションへジャンプ
1,867件の閲覧回数
Michell
Contributor I

Hello, I'm having the following problem running the code on the DSP: Error: Couldn't write applet to target. Can not read target memory at location: 0x0000000000000000.Please make sure that the chip selects are properly configured.
The CWPP response code is: CCSProtocolPlugin : CCS: Core not responding.

I'm using the correct settings for the chip because I've been using the same code for weeks, this problem started to happen out of nowhere.

0 件の賞賛
返信
1 解決策
1,810件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Can you tell us the part number you are using? There is not MC56F847, maybe it is MC56F84789 or something like that

what is the tools you are using for example CodeWarrior for MVU ver11.x?

Do you use USBTAP or Multilink Universal device?

BR

XiangJun Rong

 

元の投稿で解決策を見る

タグ(1)
0 件の賞賛
返信
1 返信
1,810件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Can you tell us the part number you are using? There is not MC56F847, maybe it is MC56F84789 or something like that

what is the tools you are using for example CodeWarrior for MVU ver11.x?

Do you use USBTAP or Multilink Universal device?

BR

XiangJun Rong

 

タグ(1)
0 件の賞賛
返信