Plug type J11/J12 Twr-K65f180m

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Plug type J11/J12 Twr-K65f180m

3,495件の閲覧回数
kevin_thomsen
Contributor I

Hello Guys,

i hope you can help me. I search the kind of connector J11/J12 (2x10 Pins) on Twr-k65f180m board. Maybe someone knows the plug type. I need the for my bachelor thesis. 

Is it a own product from nxp or a industrial standard?

pastedImage_1.png#

Thank you.

Best regards.

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

3,376件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Kevin,

It is called "Gold Finger"  or gold-plated connectors in PCB terminology.

Pls refer to the link:

Gold Fingers and Their Use in the World of PCBs – PentaLogix Blog 

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信

3,374件の閲覧回数
kevin_thomsen
Contributor I

Hi XiangJun,

thank you for your answer, but i don't mean the "Goldfinger". I mean the both black sockets on the board. 

I marked it in the picture.  

Thank you.

BR Kevin

0 件の賞賛
返信

3,374件の閲覧回数
Ben
Senior Contributor I

Hello Kevin,

If I understood your needs, you can buy connectors or cable harness that fits this card connectors. See the links:

FLE-110-01-G-DV-A Samtec Inc. | Connectors, Interconnects | DigiKey 

FFSD-10-S-06.00-01-N Samtec Inc. | Cable Assemblies | DigiKey 

0 件の賞賛
返信

3,374件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Kevin,

The connector is standard product from third party, the connector has 1.27mm pitch for the pin distance. I have checked the manufacturer.

Part number: CON 2X10 PLUG SHRD SMT 50MIL CTR 237H AU

Manufacturer: SAMTEC

Manufacturer part number: TFC-110-02-L-D-A-K

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信