PTN36043, Can I cross SS1, SS2?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PTN36043, Can I cross SS1, SS2?

1,745 次查看
Jeong
Contributor I

I plan to connect all USB SS lines using two PTN36043.
I want to use TX1 and RT2/TX2 and RX1 as a pair because the artwork design is distorted. Is there a problem with the operation when it is connected like this?
TX1 RX2 - PTN36043 #1 -
TX2 RX1 - PTN36043 #2 -

0 项奖励
回复
1 回复

1,721 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Could you please give the connection diagram?

 

0 项奖励
回复