PCA85133

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PCA85133

1,218 次查看
feiwen
Contributor I

PCA85133的VDD的输入范围为1.8-5.5V,VLCD的输入范围:2.5V-8V;请问不同的电压输入对芯片有什么影响?

0 项奖励
回复
1 回复

1,107 次查看
reyes
NXP TechSupport
NXP TechSupport

Hello,

No, there are no effects if different voltages are used to supply VDD and VLCD since they are not internally connected, VDD is used as the supply for the internal device functionality, while VLCD is the supply dedicated for pins which interface with the LCD.

 

Just take in mind that static voltages across the liquid crystal display can build up when the LCD supply voltage (VLCD) is on while the IC supply voltage (VDD) is off, or vice versa. This may cause unwanted display artifacts. To avoid such artifacts, VLCD and VDD must be applied or removed together


Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复