Hi, I am planning to use MC56F84451 and I have a problem figuring what are the functions of pins 36 and 38. The manual describes no function for pin 36 and has contradicting functions described for pin 38. I am using the document MC56F844XX.pdf (Rev. 3, 06/2014) looking at the table on page 24 and 25 where there is twice a description for pin 38 - first as GPIOE3 and then as GPIOF1 ?! (the 48 LQFP), and no description whatsoever for pin 36.
Hi, Stanko,
Pls refer to section 8.3 Signal Multiplexing and Pin Assignments in MC56F844xxRM.pdf, I copy the part here.
This is the pin assignment:
for 48 pins MC56F84451:
pin36:GPIOE3 PWMA_1A
pin38:GPIOF1 CLKO1 XB_IN7 CMPD_O
Hope it can help you
BR
XiangJun Rong