PCA85133

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCA85133

1,293件の閲覧回数
feiwen
Contributor I

PCA85133的VDD的输入范围为1.8-5.5V,VLCD的输入范围:2.5V-8V;请问不同的电压输入对芯片有什么影响?

0 件の賞賛
返信
1 返信

1,182件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hello,

No, there are no effects if different voltages are used to supply VDD and VLCD since they are not internally connected, VDD is used as the supply for the internal device functionality, while VLCD is the supply dedicated for pins which interface with the LCD.

 

Just take in mind that static voltages across the liquid crystal display can build up when the LCD supply voltage (VLCD) is on while the IC supply voltage (VDD) is off, or vice versa. This may cause unwanted display artifacts. To avoid such artifacts, VLCD and VDD must be applied or removed together


Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信