P1011NXN2DFB Specification Question

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

P1011NXN2DFB Specification Question

1,565 次查看
dannydeng
Contributor III

Can anybody provide the  Max stress  of the IC that could withstand and the Max weight the IC could withstand ?

Thanks.

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,382 次查看
LPP
NXP Employee
NXP Employee

Please, refer to AN4259 Section 27.2 Thermal Management for WB-TePBGA

"The heat sink should be attached to the printed-circuit board with the spring force centered over the center of the package. This spring force should not exceed 10 pounds of force (45 Newton)."

http://www.nxp.com/products/microcontrollers-and-processors/power-architecture-processors/qoriq-powe...

0 项奖励
回复