P1011NXN2DFB Specification Question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P1011NXN2DFB Specification Question

1,566 Views
dannydeng
Contributor III

Can anybody provide the  Max stress  of the IC that could withstand and the Max weight the IC could withstand ?

Thanks.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,383 Views
LPP
NXP Employee
NXP Employee

Please, refer to AN4259 Section 27.2 Thermal Management for WB-TePBGA

"The heat sink should be attached to the printed-circuit board with the spring force centered over the center of the package. This spring force should not exceed 10 pounds of force (45 Newton)."

http://www.nxp.com/products/microcontrollers-and-processors/power-architecture-processors/qoriq-powe...

0 Kudos
Reply