Need information regarding cell controller BMS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Need information regarding cell controller BMS

1,628 次查看
pratayay123
Contributor III

Dear Team,

As per the Application note for MC33772B Passive cell balancing also included inside the Evaluation board. please replay the below query.

1. Is it possible to get only the sensing module without the passive balancing?

2. Even if passive balancing included with the controller ..is it possible to bypass the passive balancing section?

3. is there any NXP board available for Active cell balancing?

4. Is there any module for lithium-ion battery voltage, current, and temperature sensing?

Thanks,

Pratyay

0 项奖励
回复
1 回复

1,604 次查看
guoweisun
NXP TechSupport
NXP TechSupport

For your questions the answer are NO.

0 项奖励
回复