Need information regarding cell controller BMS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Need information regarding cell controller BMS

1,692件の閲覧回数
pratayay123
Contributor III

Dear Team,

As per the Application note for MC33772B Passive cell balancing also included inside the Evaluation board. please replay the below query.

1. Is it possible to get only the sensing module without the passive balancing?

2. Even if passive balancing included with the controller ..is it possible to bypass the passive balancing section?

3. is there any NXP board available for Active cell balancing?

4. Is there any module for lithium-ion battery voltage, current, and temperature sensing?

Thanks,

Pratyay

0 件の賞賛
返信
1 返信

1,668件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

For your questions the answer are NO.

0 件の賞賛
返信