Need help to develope SPI interface on MPC 5517

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need help to develope SPI interface on MPC 5517

2,589 Views
ramakrishna_pen
Contributor I

Hello All,

 

I use MPC 5517 micro controller, I am using one of the SPI interface to communicate with Ethernet controller, Need to configure MPC 5517 SPI interface as master.

 

Can some one provide sample source code where i can modify the same for my project.

 

Any help hightly appreciated.

 

Thanks & Regards

Ram

Labels (1)
Tags (2)
0 Kudos
Reply
2 Replies

1,981 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

take a look at this application note, there's simple example directly for MPC5517:

http://www.freescale.com/files/32bit/doc/app_note/AN2865.pdf

http://www.freescale.com/webapp/sps/download/license.jsp?colCode=AN2865SW

Lukas

0 Kudos
Reply

1,981 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,ramakrishna,

Sorry for not helping you, this is DSC space rather than Qorivva space, pls create one in Qorivva space.

BR

Xiangjun Rong

0 Kudos
Reply