Need MC56F84543 Vdd power on ramp up specification/Delta

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Need MC56F84543 Vdd power on ramp up specification/Delta

跳至解决方案
3,620 次查看
LaMoris
NXP Employee
NXP Employee

Hello Richy,

 

Delta Shanghai report that MC56F84543 is latched up by a tiny ramp up voltage 0V~0.4V input to ADC pin when power on. This tiny voltage can be measured on Vdd, Reset as well, which means the system send power to Vdd later than other pins. Customer need our Vdd power on ramp up specification to modify their H/W circuit. Thanks for help.

 

Project is Baidu server power 2000W PFC, socket is MC56F84543VLH, GIBC is 1-1P4H1MP, LTR is $223.36K.

 

The signal description of waveform as below:

CH1(Yellow):GPIOA6(Pin10), used for test toggle signal. High steady means DSC does not work.

CH2(Green): Vdd.

CH3(Red): ResetB.

CH4(Blue):12V power source to Vdd 3.3V.

22648_22648.jpg84543 latched up.jpg


Best Regards,

Moris Hsu

MCU FAE


标签 (1)
标记 (3)
0 项奖励
回复
1 解答
3,247 次查看
richy_ye
NXP Employee
NXP Employee

Hi Moris, the VDD power ramp up is between 1 ms to 100 ms.

在原帖中查看解决方案

0 项奖励
回复
1 回复
3,248 次查看
richy_ye
NXP Employee
NXP Employee

Hi Moris, the VDD power ramp up is between 1 ms to 100 ms.

0 项奖励
回复