Need MC56F84543 Vdd power on ramp up specification/Delta

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need MC56F84543 Vdd power on ramp up specification/Delta

Jump to solution
1,755 Views
LaMoris
NXP Employee
NXP Employee

Hello Richy,

 

Delta Shanghai report that MC56F84543 is latched up by a tiny ramp up voltage 0V~0.4V input to ADC pin when power on. This tiny voltage can be measured on Vdd, Reset as well, which means the system send power to Vdd later than other pins. Customer need our Vdd power on ramp up specification to modify their H/W circuit. Thanks for help.

 

Project is Baidu server power 2000W PFC, socket is MC56F84543VLH, GIBC is 1-1P4H1MP, LTR is $223.36K.

 

The signal description of waveform as below:

CH1(Yellow)GPIOA6(Pin10), used for test toggle signal. High steady means DSC does not work.

CH2(Green): Vdd.

CH3(Red): ResetB.

CH4(Blue):12V power source to Vdd 3.3V.

22648_22648.jpg84543 latched up.jpg


Best Regards,

Moris Hsu

MCU FAE


Labels (1)
Tags (3)
0 Kudos
1 Solution
1,382 Views
richy_ye
NXP Employee
NXP Employee

Hi Moris, the VDD power ramp up is between 1 ms to 100 ms.

View solution in original post

0 Kudos
1 Reply
1,383 Views
richy_ye
NXP Employee
NXP Employee

Hi Moris, the VDD power ramp up is between 1 ms to 100 ms.

0 Kudos