MC56F8335 program flash size

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC56F8335 program flash size

1,449 Views
ulrichneumayer
Contributor I

Hi,

i have a question about the MC56F8335 program flash size. The technical data sheet:

http://www.nxp.com/assets/documents/data/en/data-sheets/MC56F8335.pdf

says:

* Table 4-1: Program Flash 64kB

* Table 4-4: Internal Program Flash 64kB from P:0x00 0000 to P:0x00 7FFF

I think this is wrong! The right program flash size must be 128kB (from P:0x00 0000 to P:0x 00 FFFF)

Only figure 4-1 shows the wright adress-area (P:0x00 0000 to P:0x00 FFFF) with flash configure field at P:0x00 FFF7 to P:0x00 FFFF. The text in figure 4-1 "64kB" is wrong!

 

I ordered an MC56F8335 and thougt the program flash size is 64kB. Then i erased the program flash and wrote the configure field at P:0x00 7FF7 to P:0x00 7FFF without securing the flash and without setting the protection-bits and i wondered that the DSP-Code itselfe cannot program the data flash. This is because the flash size is 128kB and the Configure field is at P:0x00 FFF7 to P:0x00 FFFF and after erasing the flash the protection-bits in the configure field are all set. So the flash is protected.

Is this correct?

 

Friendly regards,

Uli

Labels (1)
0 Kudos
Reply
1 Reply

1,246 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Uli,

You are right, the program flash is 64KW instead of 64KB, the program flash ranges from P:0x00_0000 to P:0x00_0xFFFF, obviously, it is 64KW or 128KB. So the data sheet is wrong, I will notify docmentation team of the issue.

soory for the inconvenience.

BR

Xiangjun Rong

0 Kudos
Reply