MC56F8247 Flash size is 48KB or 64KB?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC56F8247 Flash size is 48KB or 64KB?

ソリューションへジャンプ
2,449件の閲覧回数
larryyang
NXP Employee
NXP Employee


From the datasheet we can find the flash size of MC56F8247 is 48KB, but I find a customer configured it as 64KB in .cmd file. After the code is compiled, we find the actual used FLASH size exceeds 48KB in .xMAP file. Do you know whether the flash size of MC56F8247 is 48KB or 64KB?

ラベル(1)
0 件の賞賛
返信
1 解決策
2,323件の閲覧回数
johnlwinters
NXP Employee
NXP Employee

The data sheet is correct.  If any extra flash is present it would not be per the product specification; there is no assurance that such extra flash exists or will exist.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,324件の閲覧回数
johnlwinters
NXP Employee
NXP Employee

The data sheet is correct.  If any extra flash is present it would not be per the product specification; there is no assurance that such extra flash exists or will exist.

0 件の賞賛
返信