MC56F8247 Flash size is 48KB or 64KB?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC56F8247 Flash size is 48KB or 64KB?

Jump to solution
2,452 Views
larryyang
NXP Employee
NXP Employee


From the datasheet we can find the flash size of MC56F8247 is 48KB, but I find a customer configured it as 64KB in .cmd file. After the code is compiled, we find the actual used FLASH size exceeds 48KB in .xMAP file. Do you know whether the flash size of MC56F8247 is 48KB or 64KB?

Labels (1)
0 Kudos
Reply
1 Solution
2,326 Views
johnlwinters
NXP Employee
NXP Employee

The data sheet is correct.  If any extra flash is present it would not be per the product specification; there is no assurance that such extra flash exists or will exist.

View solution in original post

0 Kudos
Reply
1 Reply
2,327 Views
johnlwinters
NXP Employee
NXP Employee

The data sheet is correct.  If any extra flash is present it would not be per the product specification; there is no assurance that such extra flash exists or will exist.

0 Kudos
Reply