MC56F82323

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC56F82323

2,871件の閲覧回数
antonio66
Contributor III

Hi,

the MC56F82323 has two or three Comparators on ADC inputs ?

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

2,595件の閲覧回数
antonio66
Contributor III

Because,

on MC56F823XX.pdf and on MC56F823XXRM.pdf is writed:

pastedImage_0.png

But on Processor Expert and in DSC56800EX_Quick_Start there are 3 comp !

0 件の賞賛
返信

2,595件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

The information on our documents (Data Sheet and Reference Manual) is correct.

What is the CodeWarrior version you are using? MC56F82323 is not supported by Processor Expert in CodeWarrior v10.6.2. And I checked in CW10.6.3, it is not supported either. Could you please send me a screenshot to show the Processor List in Components Library like below?

pastedImage_0.png


Thank you very much!

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

2,595件の閲覧回数
antonio66
Contributor III

pastedImage_0.png

0 件の賞賛
返信

2,595件の閲覧回数
antonio66
Contributor III

Hi,

Sorry youa are right: in the processor expert i used the MC56F82723.

but on manual

pastedImage_1.png

But in the Quick_Start:

pastedImage_0.png

0 件の賞賛
返信

2,595件の閲覧回数
mohammad_kamil
NXP Employee
NXP Employee

Thanks Antonio, we will look into this and confirm.

0 件の賞賛
返信