MC56F82323

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC56F82323

3,024 Views
antonio66
Contributor III

Hi,

the MC56F82323 has two or three Comparators on ADC inputs ?

Labels (1)
0 Kudos
Reply
5 Replies

2,748 Views
antonio66
Contributor III

Because,

on MC56F823XX.pdf and on MC56F823XXRM.pdf is writed:

pastedImage_0.png

But on Processor Expert and in DSC56800EX_Quick_Start there are 3 comp !

0 Kudos
Reply

2,748 Views
TICS_Fiona
NXP Employee
NXP Employee

The information on our documents (Data Sheet and Reference Manual) is correct.

What is the CodeWarrior version you are using? MC56F82323 is not supported by Processor Expert in CodeWarrior v10.6.2. And I checked in CW10.6.3, it is not supported either. Could you please send me a screenshot to show the Processor List in Components Library like below?

pastedImage_0.png


Thank you very much!

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

2,748 Views
antonio66
Contributor III

pastedImage_0.png

0 Kudos
Reply

2,748 Views
antonio66
Contributor III

Hi,

Sorry youa are right: in the processor expert i used the MC56F82723.

but on manual

pastedImage_1.png

But in the Quick_Start:

pastedImage_0.png

0 Kudos
Reply

2,748 Views
mohammad_kamil
NXP Employee
NXP Employee

Thanks Antonio, we will look into this and confirm.

0 Kudos
Reply