Is there a sample project for the MC56F84789 device that illustrates use of STOP instruction? (Yes, and I include this below)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there a sample project for the MC56F84789 device that illustrates use of STOP instruction? (Yes, and I include this below)

1,469件の閲覧回数
johnlwinters
NXP Employee
NXP Employee

Yes, the halt and wait are illustrated in the attached zip file which is a zipped project for CodeWarrior 10.6.

It runs on the Tower module for the MC56F84789.

 

Note, most of the work is done with the GUI and Processor Expert.

 

Note that since I used a timer, I can make this time stop or keep running in PEx depending on how I configure the CPU component.

 

Right now, it is set for keep running.

 

Can you make it STOP during STOP mode?

Original Attachment has been moved to: Haltish.zip

ラベル(1)
0 件の賞賛
返信
0 返答(返信)