How to use PESL (Processor Expert Software Library) without generating compile errors - here's how:

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to use PESL (Processor Expert Software Library) without generating compile errors - here's how:

1,866 次查看
johnlwinters
NXP Employee
NXP Employee

To avoid errors, rename the peripheral initialization component to a unique name!  That's it!

 

 

 

This is done by first

 

--adding the inialization component, selecting advanced at the upper right, and then

 

 

--editing the name which is the first property of the component. You can for example add "my" as a suffix.

 

Then, you can use the PESL commands by dragging them in without generating compile errors.

 

(The root cause of this is a name space collision between header files generated by PESL usage and PEx generated code.  But, you don't need worry about it if you do the above work-a-round.)

标签 (1)
标记 (2)
0 项奖励
回复
0 回复数