How to use PESL (Processor Expert Software Library) without generating compile errors - here's how:

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use PESL (Processor Expert Software Library) without generating compile errors - here's how:

1,879 Views
johnlwinters
NXP Employee
NXP Employee

To avoid errors, rename the peripheral initialization component to a unique name!  That's it!

 

 

 

This is done by first

 

--adding the inialization component, selecting advanced at the upper right, and then

 

 

--editing the name which is the first property of the component. You can for example add "my" as a suffix.

 

Then, you can use the PESL commands by dragging them in without generating compile errors.

 

(The root cause of this is a name space collision between header files generated by PESL usage and PEx generated code.  But, you don't need worry about it if you do the above work-a-round.)

Labels (1)
Tags (2)
0 Kudos
Reply
0 Replies