Hi, We are using MSC8122 star core DSP in out product. Due to redesign, We have to do Signal Intigrity for TDM interface. The IBIS model given is "iopad_h8_s_iod" in the IBIS file io_8122_rev0_3_1.ibs, but this is not giving expexted results. Can some one

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Hi, We are using MSC8122 star core DSP in out product. Due to redesign, We have to do Signal Intigrity for TDM interface. The IBIS model given is "iopad_h8_s_iod" in the IBIS file io_8122_rev0_3_1.ibs, but this is not giving expexted results. Can some one

1,381 次查看
kranthiracha
Contributor I

Hi,

We are using MSC8122 star core DSP in out product. Due to redesign, We have to do Signal Intigrity for TDM interface. The IBIS model given is "iopad_h8_s_iod" in the IBIS file io_8122_rev0_3_1.ibs, but this is not giving expexted results. Can some one tell me which IBIS model should be used for TDM Tx and Rx signals

标签 (1)
0 项奖励
回复
2 回复数

1,081 次查看
lunminliang
NXP Employee
NXP Employee

Hello Kranthi racha,

Please provide more information about given result vs measured. What SI tool do you use and load model in simulation.

Regards

Lunmin

0 项奖励
回复

1,081 次查看
johnlwinters
NXP Employee
NXP Employee

This group does not include the Star*Core.  That is not a digital signal controller, it is used mainly for telecomunications.

0 项奖励
回复