Hi, We are using MSC8122 star core DSP in out product. Due to redesign, We have to do Signal Intigrity for TDM interface. The IBIS model given is "iopad_h8_s_iod" in the IBIS file io_8122_rev0_3_1.ibs, but this is not giving expexted results. Can some one

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hi, We are using MSC8122 star core DSP in out product. Due to redesign, We have to do Signal Intigrity for TDM interface. The IBIS model given is "iopad_h8_s_iod" in the IBIS file io_8122_rev0_3_1.ibs, but this is not giving expexted results. Can some one

1,370 Views
kranthiracha
Contributor I

Hi,

We are using MSC8122 star core DSP in out product. Due to redesign, We have to do Signal Intigrity for TDM interface. The IBIS model given is "iopad_h8_s_iod" in the IBIS file io_8122_rev0_3_1.ibs, but this is not giving expexted results. Can some one tell me which IBIS model should be used for TDM Tx and Rx signals

Labels (1)
0 Kudos
Reply
2 Replies

1,070 Views
lunminliang
NXP Employee
NXP Employee

Hello Kranthi racha,

Please provide more information about given result vs measured. What SI tool do you use and load model in simulation.

Regards

Lunmin

0 Kudos
Reply

1,070 Views
johnlwinters
NXP Employee
NXP Employee

This group does not include the Star*Core.  That is not a digital signal controller, it is used mainly for telecomunications.

0 Kudos
Reply