Does the Eclipse version of Codewarrior support for the 56F8367?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does the Eclipse version of Codewarrior support for the 56F8367?

1,468 Views
LesleyF
Contributor I

We are using the DSP 56F8367 in a number of products.  We want to switch to the Ecplipse version of Codewarrior.  Does it support this MCU?

 

Thanks!

Labels (1)
0 Kudos
Reply
3 Replies

1,309 Views
dynapb
Contributor IV

Hi Lesley

I have used the 56F8367 processor for a project and used the Classic CW for it.  Now I am using a new procesor that Classic does not support so am using Eclipse based CW.  It is nice to use in general but it is very slow compared to Classic.  Have you used the Eclipse version yet and is that what you find?

Thanks

Pete

0 Kudos
Reply

1,309 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Yes, the Eclipse vresion of CodeWarrior  called CodeWarrior for mcu ver10.6 or ver10.7 supports MC56F83xx family.

Hope it can help you

BR

Xiangjun Rong

0 Kudos
Reply

1,309 Views
LesleyF
Contributor I

Thanks Xianjun.  That is helpful information.

0 Kudos
Reply