Do the input pins have Schmitt Trigger before signal goes elsewhere on MC56F82746?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Do the input pins have Schmitt Trigger before signal goes elsewhere on MC56F82746?

Jump to solution
1,618 Views
dynapb
Contributor IV

I need a Schmitt trigger on a XBARB input that is routed from a "Package Pin" and to the AOI module.

I cannot tell by the pin diagram in MC56F827XXRM if the Pin Inputs have a Schmitt trigger on them before the signal goes to the XBARB inputs or not?

174103_174103.pngGPIO_LogicDiagram.png

Does the XBARB get signals from RAWDATA or from the On-Chip Peripheral signals (that might have the Schmitt trig)?

This is probably a question for a chip internals guru.

Thanks for any insights,

Pete

Labels (1)
0 Kudos
Reply
1 Solution
1,334 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

External pin connects to I/o pad, I/o pad connects to gpio and xbar and other peripherals.  Schmitt is in I/o pad. So all digital inputs have the same behavior.

Hope it can help you

BR

XiangJun Rong

View solution in original post

0 Kudos
Reply
1 Reply
1,335 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

External pin connects to I/o pad, I/o pad connects to gpio and xbar and other peripherals.  Schmitt is in I/o pad. So all digital inputs have the same behavior.

Hope it can help you

BR

XiangJun Rong

0 Kudos
Reply