Do the input pins have Schmitt Trigger before signal goes elsewhere on MC56F82746?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Do the input pins have Schmitt Trigger before signal goes elsewhere on MC56F82746?

跳至解决方案
1,759 次查看
dynapb
Contributor IV

I need a Schmitt trigger on a XBARB input that is routed from a "Package Pin" and to the AOI module.

I cannot tell by the pin diagram in MC56F827XXRM if the Pin Inputs have a Schmitt trigger on them before the signal goes to the XBARB inputs or not?

174103_174103.pngGPIO_LogicDiagram.png

Does the XBARB get signals from RAWDATA or from the On-Chip Peripheral signals (that might have the Schmitt trig)?

This is probably a question for a chip internals guru.

Thanks for any insights,

Pete

标签 (1)
0 项奖励
回复
1 解答
1,475 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

External pin connects to I/o pad, I/o pad connects to gpio and xbar and other peripherals.  Schmitt is in I/o pad. So all digital inputs have the same behavior.

Hope it can help you

BR

XiangJun Rong

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,476 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

External pin connects to I/o pad, I/o pad connects to gpio and xbar and other peripherals.  Schmitt is in I/o pad. So all digital inputs have the same behavior.

Hope it can help you

BR

XiangJun Rong

0 项奖励
回复