Debugger for MC56F81666 VLH DSC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debugger for MC56F81666 VLH DSC

2,543件の閲覧回数
AnanthuRG
Contributor I

Can anybody help me to use which debugger for MC56F81XXX series DSC cards

I am using MC56F81666 from this family, I am also planning to buy the development board from this series which is MC56F8x series.

I am confused about which debugger (emulator) to use for the flashing the code.

 

0 件の賞賛
返信
3 返答(返信)

2,536件の閲覧回数
AnanthuRG
Contributor I

Thank you for the response.

Is there any other options other than using universal multilink probe as a debugger?

any affordable one? I am using this for DSC only

0 件の賞賛
返信

2,535件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

At the time being, the Multilink Universal device from third party is the only option as a debugger for MC56F81xxx and MC56F83xxx DSC families.

www.pemicro.com

BR

Xiang Jun Rong

0 件の賞賛
返信

2,539件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

This is MC56F81xxx link:

https://www.nxp.com/products/processors-and-microcontrollers/additional-mpu-mcus-architectures/digit...

 

You can download the CodeWarrior for MCU ver11.x tools from the link:

https://www.nxp.com/design/software/development-software/codewarrior-development-tools/codewarrior-l...

 

You have to order the third party Multilink Universal device from the PE micro company

www.pemicro.com

The USBTAP device is NOT supported for MC56F81xxx and MC56F83xxx.

With the CodeWarrior for MCU ver11.x tools  plus the Multilink Universal device, you can download application code to flash and debug for MC56F81xxx and MC56F83xxx.

Hope it can help you

BR

XiangJun Rong

 

0 件の賞賛
返信