Dataseet saf7730

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Dataseet saf7730

6,565 Views
lysyhaleksandr
Contributor I

Hello! I can’t find a datasheet for saf 7730 anywhere! Can anyone have information?

0 Kudos
Reply
4 Replies

6,481 Views
guoweisun
NXP TechSupport
NXP TechSupport

This product had already EOL now!

0 Kudos
Reply

5,681 Views
Nickldio
Contributor I

I also need the datasheet for the SAF7730HV, I found one for the SAF7741. Are they similar enough to work with that instead? I'm looking for the I2C registers to switch the input to SPDIF.

0 Kudos
Reply

6,058 Views
galaxy_110
Contributor II

Also I need a datasheet of saf7730

6,252 Views
Dunconi
Contributor I

I would be grateful if a datasheet for the SAF7730HV/233 were to be made available. I appreciate that the part is EOL, but there is still equipment in the field that requires servicing and repair. I would be surprised if this request was blocked on the grounds of IP when the part is EOL and was designed around 15-years ago.