Can try operate a 90V voltage in mc33816?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can try operate a 90V voltage in mc33816?

Jump to solution
2,093 Views
kangdaecheol
Contributor I

 

hello.


I have a question about mc33816.


I try use SOGAV at mc33816.


but SOGAV need a 90V boost voltage.


So I try to use 90V Voltage in mc33816.


Can it operate without problem when to use 90V voltage in mc33816?


If threre are some problem, would you let me know that?

 

Labels (1)
0 Kudos
Reply
1 Solution
1,893 Views
johnlwinters
NXP Employee
NXP Employee

The device you mention is a Programmable solenoid controller, and is not a subject of this particular forum.

Please contact the helpdesk directly with this question.

View solution in original post

0 Kudos
Reply
1 Reply
1,894 Views
johnlwinters
NXP Employee
NXP Employee

The device you mention is a Programmable solenoid controller, and is not a subject of this particular forum.

Please contact the helpdesk directly with this question.

0 Kudos
Reply