Can try operate a 90V voltage in mc33816?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can try operate a 90V voltage in mc33816?

ソリューションへジャンプ
2,073件の閲覧回数
kangdaecheol
Contributor I

 

hello.


I have a question about mc33816.


I try use SOGAV at mc33816.


but SOGAV need a 90V boost voltage.


So I try to use 90V Voltage in mc33816.


Can it operate without problem when to use 90V voltage in mc33816?


If threre are some problem, would you let me know that?

 

ラベル(1)
0 件の賞賛
返信
1 解決策
1,873件の閲覧回数
johnlwinters
NXP Employee
NXP Employee

The device you mention is a Programmable solenoid controller, and is not a subject of this particular forum.

Please contact the helpdesk directly with this question.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,874件の閲覧回数
johnlwinters
NXP Employee
NXP Employee

The device you mention is a Programmable solenoid controller, and is not a subject of this particular forum.

Please contact the helpdesk directly with this question.

0 件の賞賛
返信