Can't download program to flash on MC56F8

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can't download program to flash on MC56F8

4,290件の閲覧回数
sm0khey
Contributor III

Hello guys!

I am using CodeWarrior with UTAP for flashing the MCU. The problem i encounter is the following:

sm0khey_1-1718620887209.pngsm0khey_1-1718620887209.png

 

sm0khey_0-1718620862351.pngsm0khey_0-1718620862351.png

Also when i use the software for flashing with UTAP, i get the error :

Performing PROGRAM operation on MC56F8257 through the UTAP . . .
HawkV2: Core not responding

Also i can connect to the MCU and use the old version of the software.
I saw that i might have locked the flash, but nothing has worked so far. Any idea how to fix this?
It happened to 2 MCU's so far

タグ(5)
0 件の賞賛
返信
5 返答(返信)

4,200件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I do not know if the usbtap device is okay or not.

This is the usbtap for once.

https://www.nxp.com/products/processors-and-microcontrollers/additional-mpu-mcus-architectures/digit...

 

You can also use multilink universal from third party:

www.pemicro.com

I suppose you use your own PCB board, is your PCB board okay?

BR

XiangJun Rong

4,198件の閲覧回数
sm0khey
Contributor III

Yes, my PCB board is ok, i've tried on 3 more boards and still says that you cannot connect to the core. I believe it's a problem with the USBTap, but i can't seem to fix it

0 件の賞賛
返信

4,186件の閲覧回数
sm0khey
Contributor III

Turns out the problem is not in my USBTap. I've tried to download another .elf to another DSC and it worked, but still cannot flash the first 3 DSC's. Any idea what might be the problem? The program i wanted to flash included commands to delete blocks of flash memory. Could i have locked the MCU? Also i can still control the digital inputs/outputs of the DSC controller that i can't download a new flash.

Also:

sm0khey_0-1719412105289.pngsm0khey_0-1719412105289.png


When i restart the DSC still won't connect

タグ(1)
0 件の賞賛
返信

4,272件の閲覧回数
sm0khey
Contributor III

up

0 件の賞賛
返信

4,223件の閲覧回数
sm0khey
Contributor III

up

0 件の賞賛
返信