Can I use a MC56F8257 code to a MC56F82748?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I use a MC56F8257 code to a MC56F82748?

1,450 Views
kienfrancis_ure
Contributor II

Can I use a MC56F8257 code to a MC56F82748? I got a sample code from the MC56F8257 of eFlexPWM and yet I want to know if I need to adjust the code?

Tags (2)
0 Kudos
Reply
4 Replies

1,360 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Kien,

The eFlexPWM module is the same for MC56F8257 and MC56F82748, so the eFlexPWM code for MC56F8257 is also valid for MC56F82748. But I think the clock and pin assignment are different.

Pls download sample code of MC56F82748 from the link:

MC56F827xx Example Code 

The example code includes the eFlexPWM example.

Hope it can help you

BR

Xiangjun Rong

0 Kudos
Reply

1,360 Views
kienfrancis_ure
Contributor II

Thank you. But I want to know to what document should I use as reference in

MC56F82748? I cant find any reference manual. Thanks

On Tue, Mar 26, 2019, 11:28 AM xiangjun.rong <admin@community.nxp.com>

0 Kudos
Reply

1,360 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Pls download the reference manual of MC56F82748 from the link:

https://www.nxp.com/docs/en/reference-manual/MC56F827XXRM.pdf 

Pls download data sheet from the link:

https://www.nxp.com/docs/en/reference-manual/MC56F827XXRM.pdf 

Hope it can help you

BR

XiangJun Rong

0 Kudos
Reply

1,360 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Kien,

Pls download the reference manual and data sheet of MC56F827xx from the link:

MC56F82xxx | NXP 

BR

Xiangjun Rong

0 Kudos
Reply