C8051F38/B-GQ and C2 programming

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

C8051F38/B-GQ and C2 programming

1,513件の閲覧回数
pzpz
Contributor I

Hello,

I am making one USB model using C8051F38/B-GQ.

I have designed the circuit and want to program it using serial adapter EC2.

I selected C2 ad debug interface and EC2 serial adapter with port and baudrate.

I tried to connect the controller board with EC2 but it is not connecting.
my whole system is running on 5Vsupply but for programming I am using 3.3V which is generated by controller itset at pin 6 ie VDD.
Please reply so that I can discuss further issues and circuit for guidance

Regards

pzpz

ラベル(1)
0 件の賞賛
返信
1 返信

1,340件の閲覧回数
johnlwinters
NXP Employee
NXP Employee

This device falls outside the scope of this community forum.

0 件の賞賛
返信