C8051F38/B-GQ and C2 programming

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

C8051F38/B-GQ and C2 programming

1,620 次查看
pzpz
Contributor I

Hello,

I am making one USB model using C8051F38/B-GQ.

I have designed the circuit and want to program it using serial adapter EC2.

I selected C2 ad debug interface and EC2 serial adapter with port and baudrate.

I tried to connect the controller board with EC2 but it is not connecting.
my whole system is running on 5Vsupply but for programming I am using 3.3V which is generated by controller itset at pin 6 ie VDD.
Please reply so that I can discuss further issues and circuit for guidance

Regards

pzpz

标签 (1)
0 项奖励
回复
1 回复

1,447 次查看
johnlwinters
NXP Employee
NXP Employee

This device falls outside the scope of this community forum.

0 项奖励
回复