56F8367EVM Program Error using ONCE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

56F8367EVM Program Error using ONCE

3,018 次查看
estevenzhu
Contributor I

trying to program the EV board (P/N: 56F8367EVM ),  however, always have problem, anyone can help?

Hardware:   MC56F8367EVM 

Programmer:  CodeWarrior USB TAP , ONCE

Computer: Win 10. 

CodeWarrior, 8.2.3  and 11 (Latest Download)

Error:  Executing task MC56F8367

Error: Couldn't write applet to target. Can not read target memory at location: 0x 0000000000000FC00.  please make sure that the chip select are properly configured. 

 

We checked all jumper settings.   JG3, is shorted instead of open.  Do we need to change other jumpers?   Or what should we do?     

0 项奖励
回复
3 回复数

3,003 次查看
Ben
Senior Contributor I

we had a lot of problems using ONCE on the 56F8367 chip. PEmicro multilink universal works perfect.

Ben

0 项奖励
回复

3,000 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Ben,

Okay, pls use multilink universal device to download/debug the MC56F8367 board.

BR

XiangJun Rong

0 项奖励
回复

3,007 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

There is issue if you use CodeWarrior for DSP56800E ver8.x on Win10, I suggest you use CodeWarrior for MCU ver11.x, which supports MC56F8367 and Win10 OS.

https://www.nxp.com/design/software/development-software/codewarrior-development-tools/codewarrior-l...

If you still have issue, you can use multilink universal device from PEmicro

www.pemicro.com

Hope it can help you

BR

XiangJun Rong

 

0 项奖励
回复