56F8367EVM Program Error using ONCE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

56F8367EVM Program Error using ONCE

3,159 Views
estevenzhu
Contributor I

trying to program the EV board (P/N: 56F8367EVM ),  however, always have problem, anyone can help?

Hardware:   MC56F8367EVM 

Programmer:  CodeWarrior USB TAP , ONCE

Computer: Win 10. 

CodeWarrior, 8.2.3  and 11 (Latest Download)

Error:  Executing task MC56F8367

Error: Couldn't write applet to target. Can not read target memory at location: 0x 0000000000000FC00.  please make sure that the chip select are properly configured. 

 

We checked all jumper settings.   JG3, is shorted instead of open.  Do we need to change other jumpers?   Or what should we do?     

0 Kudos
Reply
3 Replies

3,144 Views
Ben
Senior Contributor I

we had a lot of problems using ONCE on the 56F8367 chip. PEmicro multilink universal works perfect.

Ben

0 Kudos
Reply

3,141 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Ben,

Okay, pls use multilink universal device to download/debug the MC56F8367 board.

BR

XiangJun Rong

0 Kudos
Reply

3,148 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

There is issue if you use CodeWarrior for DSP56800E ver8.x on Win10, I suggest you use CodeWarrior for MCU ver11.x, which supports MC56F8367 and Win10 OS.

https://www.nxp.com/design/software/development-software/codewarrior-development-tools/codewarrior-l...

If you still have issue, you can use multilink universal device from PEmicro

www.pemicro.com

Hope it can help you

BR

XiangJun Rong

 

0 Kudos
Reply