求《AN4813:Encoder Position and Speed Sensing Utilizing the Quad Timer on the MC56F827xx DSCs》这篇文章的工程附件

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

求《AN4813:Encoder Position and Speed Sensing Utilizing the Quad Timer on the MC56F827xx DSCs》这篇文章的工程附件

1,677件の閲覧回数
建雄惠
Contributor I

求《AN4813:Encoder Position and Speed Sensing Utilizing the Quad Timer on the MC56F827xx DSCs》这篇文章的工程附件。带详细程序的工程附件。

谢谢!

ラベル(1)
0 件の賞賛
返信
1 返信

1,502件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello

The application example code is already included in the pdf document.  It is extracted from the project for our customer, so we cannot send the full project to you. 

However, all the code lines used in the context of this application has been given in the document.

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信