will i.MX27's some USART(1-2 of 6)  add ISO7816 smartcard support like ATMEL does?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

will i.MX27's some USART(1-2 of 6)  add ISO7816 smartcard support like ATMEL does?

2,822 次查看
Stven
Contributor I
I have review i.MX27's spec, it is a good chip to dev a new high-end embedded EFTPOS, please do some work to support ISO7816 smartcard standard!  eg. ATMEL AT91SAMs add 7816 compatible UART function to exist standard USARTs, it is not difficult but useful!  If tapout a i.MX27L/S to drop H.264/H.263/ cameraI/F is so good, don't forgot big-pitch package to support six-layer PCB & industry temp range.
标签 (1)
0 项奖励
回复
1 回复

872 次查看
Stven
Contributor I
also 8*8 keyboard support is so limited, think about 8*12-16
0 项奖励
回复