will i.MX27's some USART(1-2 of 6)  add ISO7816 smartcard support like ATMEL does?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

will i.MX27's some USART(1-2 of 6)  add ISO7816 smartcard support like ATMEL does?

2,819 Views
Stven
Contributor I
I have review i.MX27's spec, it is a good chip to dev a new high-end embedded EFTPOS, please do some work to support ISO7816 smartcard standard!  eg. ATMEL AT91SAMs add 7816 compatible UART function to exist standard USARTs, it is not difficult but useful!  If tapout a i.MX27L/S to drop H.264/H.263/ cameraI/F is so good, don't forgot big-pitch package to support six-layer PCB & industry temp range.
Labels (1)
0 Kudos
Reply
1 Reply

869 Views
Stven
Contributor I
also 8*8 keyboard support is so limited, think about 8*12-16
0 Kudos
Reply