using an 8-bit LCD with the MCF52230

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

using an 8-bit LCD with the MCF52230

2,386件の閲覧回数
baddad
Contributor I
Has anyone succefully used an 8-bit LCD with the MCF52230?
 
If so, do you have any tips, tricks or code examples you would be willing to share?
 
Best Regards,
BadDad
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

900件の閲覧回数
mjbcswitzerland
Specialist V
Note that there is an online demo of LCD control at

LCD control

It can be seen by web cam at WEB CAM

At the control link there is also a stand-alone LCD (and key board) simulator which can be downloaded (called VIPpanel). This is not M52230 specific but does enable control of a web-based LCD as well as practical testing of all LCD functionality - full documentation is included in the simulator.

Regards

0 件の賞賛
返信

900件の閲覧回数
mjbcswitzerland
Specialist V
Hi BadDad

Take a look at the uTasker project.
It includes LCD support, including an LCD simulator.
See www.uTasker.com

regards

Mark Butcher

0 件の賞賛
返信