updated BSP for m54455evb?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

updated BSP for m54455evb?

1,959件の閲覧回数
JimDouglas
Contributor I
I am using the m54455evb BSP, dated 20071214. 
 
I see from the release notes that there are a number of known issues.  Specifically, Bug 858: ethernet performance, Bug 972: uart dma, Bug 974: hrtimer disabled. 
 
Are there any plans to resolve these issues? 
 
Also, has anyone attempted to upgrade this kernel from 2.6.23 to 2.6.23.17?  I patched it without problems, but have not tested it fully. 
 
--jim
ラベル(1)
0 件の賞賛
返信
1 返信

1,136件の閲覧回数
kmahan
Contributor I
Jim,

There are definitely plans to resolve these issues (and others).  Currently there isn't a definitive date for the release of an updated BSP.

As for upgrading to 2.6.23-17 -- I haven't tried but I'm not aware of anything that should break.

--Kurt
0 件の賞賛
返信